This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243-Q1: Outputs state when driver is not powered

Part Number: DRV8243-Q1

Hi,

I would like to know outputs state when driver is not powered. Indeed, datasheet indicates that driver outputs are in Hi-Z when for example SLEEP pin is active but I didn't find any information about outputs state when driver is not powered.

I would like to prevent any board auto-powering in case of regeneration if motor is moved manually on my system. I would eventualy avoid that by placing a diode (or other protection) on H-bridge power path but this takes some space on my board...

Thanks.

Best regards,

  • Hi Paul,

    Thank you for your post. While the driver is not powered the FETs would not have any drive and the bridge FETs would be Hi-Z. However the MOSFETs have body diodes as these are inherent in their structures. These body diodes would conduct the motor generated output back to the VM when the motor is moved manually. This will be true for discrete MOSFEts based H-bridges as well. 

    Regards, Murugavel 

  • Hi Murugavel,

    First, thanks for you answer.

    You're right, I didn't think to MOSFET themselves and their integrated diodes that run as classic H-bridge.

    So, I don't have really choice to avoid auto-powering, I must place something to block reverse current. I think to use an ideal diode controller (ex: LM74700) placed in series with H-bridge power path and eventualy combine it with a braking resistor to dissipate regeneration energy on bridge side. Do you think it would be suitable? Thanks.

    Best regards,

  • Hi Paul,

    Yes I have seen customers do similar schemes to avoid auto-powering. You want to consider auto-powering proving VM to the DRV. Be sure to have the driver disabled using DRVOFF  Braking resistor mostly dissipates the energy to avoid any VM powering with proper sizing.

    Regards, Murugavel. 

  • Hi Murugavel,

    Okay, thanks for you return and warning for implementation.

    Best regards,