This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245-Q1: Using both outputs simultaneously in independent mode with different loads

Part Number: DRV8245-Q1


Hello Application Team,

Are there any restrictions to use the outputs of a DRV8245 in independent mode when one load is connected HighSide and the other LowSide?

Thanks,

Heinrich Reger

  • Hello Heinrich,

    While in independent mode the two half-bridges are separate. There is one caveat though. One IPROPI is shared between the two half-bridges. And current sensing is available only for the low side load. So Itrip and associated functionality with IPROPI will be available only for the half-bridge that will have low side load. For the bridge with high side load IPROPI does not sense current. Thanks.

    Regards, Murugavel