Other Parts Discussed in Thread: DRV8434S
Hi team,
My customer has several questions when using DRV8434A.
1. One of the parameters used in calculating full-scale current is TRQ_DAC. I didn't find a definition in the datasheet, can you show me the definition?
2. In the working mode and stall detection mode marked in green below, is it necessary to perform a learning mode whenever the chip is reset? Can the stall threshold data be saved when the device powered-off?

3. The stall threshold mode (circled in yellow) mentions apply threshold to TRQ_CNT/STL_TH pin. The threshold voltage that needs to be applied the TRQ_CNT/STL pin is a threshold below the red box, and has nothing to do with the output threshold from the learning mode in the green box. Am I right?
4. As the blue line is crossed, it seems that only the rightmost working mode does not need to actively stall the motor. So is it possible to determine the threshold for the yellow circle at the design stage? Or does this threshold have to be calibrated for each motor during production?

Regards,
Peter