This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCT8329A: Question about motor starting in default condition

Part Number: MCT8329A
Other Parts Discussed in Thread: MCT8329EVM

Hello, recently I'm trying to utilize the MCT8329A BLDC driver IC.

I just made a cheap development board for the IC, and all I wanna do as now is just driving the motor just for ease "without" I2C communication.

I read the manual(with the manual for MCT8329EVM too) and the default condtion for driving the motor with MCT8329A is "analog input mode" as I know.

So I tried to pull down the SPEED/WAKE pin low and applied analog voltage to DACOUT/SPEED_ANA pin but It didn't work.

I checked the PVDD, GVDD, DVDD and those are 25V, around 12V, around 2.5V.

So I guess there are some kind of problem in DVDD(since DVDD should be around 3.3V) but maybe there would be another problem.

Can anybody give me advice about this problem? I attached the circuit of my development board.

Thank you.