Hi Team,
In datasheet, it is said that the two pins SRC12 and SRC34 of DRV8844 can be connected to external current-limiting resistors, but there is no further specific explanation. Could you possibly help below questions:
1. Is the voltage that triggers the current limiting protection 0.6V?
2. Will OCP be triggered after current limiting protection is triggered?
3. Is the peak current limited or the RMS current limited?
Regards,
Annie