This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10987: Motor startup issue in -40 degrees Celsius.

Part Number: DRV10987

Hi,

We integrated the DRV10987 component into our PCB.
The DRV10987 works great, but we have a problem when testing the circuit and the motor in a climate chamber at a temperature of -40 degrees Celsius,
At this temperature the Driver fails to overcome small stuck in the motor(as a result of the low temperature).
What is the recommended solution to make the driver overcome these "mechanical problems"?

(Tested with a driver that works with sensors, there was no "mechanical problem" with the motor).