Other Parts Discussed in Thread: MCF8315C, MCF8316C-Q1
Hi Team,
My customer is using MCF8316AEVM to drive their motor and they have few doubts in that. They plan to use the 3 phase BLDC motor to do position control of the
motor using encoder feedback. They want to interface these encoder signals to the micro controller MSP430FR2355 available on board .
Kindly help clarify the below :
1. There is a requirement for implementing a position control
mechanism using sensored field oriented control in this evaluation
module by taking the outputs from an optical encoder (sine , cos and
Reference signals) so is there a possibility for doing the same.
2. Is the MSP430FR2355 micro controller Capable of taking the
encoder inputs and processing it for position control or an external
microcontroller is required for the same. If the inbuilt
microcontroller is used, is there any possibility on how it can be
re-programmed for the specified applications.
3. A normal sensorless field oriented control was implemented on a
3 phase BLDC Motor using GUI of 8316A but once the parameters are
estimated , the motor stops rotating what should be done for a
continuous rotation for the specified speed.
Thanks,
Jash