Hello sir,
Thank you for your support. My name is Oishi.
I would like to ask about the maximum output value [W] regarding the specifications of the BOOSTXL-DRV8305.
When we made an inquiry in the past, we received a reply that "there is no specific power rating, and it is designed to achieve a current drive capability of 15A RMS (20A peak)."
It is said that up to 45 V can be applied as a specification of this board, but is it correct to understand that it can output up to 900 W (45 [V]× 20 [A]) as a three-phase output from the driver to the motor?
We apologize for the inconvenience, but thank you.