This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: 3-phase PMSM GaN Inverter

Expert 1225 points
Part Number: DRV8305


Hello,

so far in my project I used TMS320, DRV8305 and discrete Si MOSFET transistors 3-phase H bridge.

But now for my client I need to go for 40kHz switching, hence I am considering GaN FETs.

But i want to configure my current project (based on Si MOSFET) in minimal possible way.

Does TI have replacement for DRV drivers that can be used with GaNs?

Also, do I need to add additional paralell diode to GaN transistor in motor control inverter application?

My application requires 60V, 100A. Does TI have suitable GaN transistors?

Regards,

Adam