Hi,
I have a board with the DRV8353SRTAT chip. I am looking at the current sense output, and it is outputting approximately 25% of Vref signal (expecting 50% of the Vref signal).
Voltages as checked:
- Vref has been checked as 3.3V.
- The voltage across the input pins SPC to SNC is checked as 0V
- The voltage of the output is ~900mV (should be 1.65V)
Can you recommend next steps for troubleshooting?