Other Parts Discussed in Thread: DRV8876
I have questions about the operation of two types of motor drivers, DRV8873 and DRV8876.
I am considering the above driver in the device currently under design.
As for control, we are considering operation at logic level by GPIO.
The “nSLEEP” and “disable” pins should be logically fixed because I/O of the CPU is insufficient.
If the “nSLEEP” and “disable” pins are fixed and the ph/EN control mode is set, the brake is the only way to stop the motor.
If possible, we would like to use the output as a Hi-Z state instead of a brake like a stop.
Therefore, in PWM control mode, “nSLEEP” and “disable” pins can be set to Hi-Z state by only logic change of the control line (IN1, IN2) with fixed pins. (Even if the speed change is required during the evaluation of the actual machine, the PWM mode can be supported, so it is also an insurance.)
Is this possible? (DRV8873 states that 100% duty is acceptable.)