Hi,
Thermal pad solder issue. When the steel plate thickness is 0.12mm, the opening size is 2.9*4.7mm.
The height will be due to the large opening area, and the solder paste in the middle will be about 107um lower than the thickness of the steel plate.
The volume will be about 85% due to height. Do you have any suggestions on how much required volume should be achieved?
The gap between EPAD and pin is 0.05mm~0.15mm. Is there a normal distribution diagram?
Follow recommend of TI spec , tin beads will appear after production. Are there any other good suggestions?
Thanks & best regards,