This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External pull up resistor for EN pin - UC27444-Q1



Hi,

We're using UC27444-Q1 for one of our applications. As per the datasheet, the EN pins are pulled up to VDD using 100k ohms. In our application, we're using certain circuitry to turn OFF the UC27444-Q1 in case of over current fault. In this case, an external pull up to EN (eg: 10k) would be an overdo ??

Thanks in advance.

Best Regards,

Prahaladh S