Hi team,
Does DRV8711 can replace L6482HTR directly in functionally? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Yes it can replace it functionally. Keep in mind the DRV8711 operating voltage is 8 V to 52 V. The L6482HTR is VSREG to 85 V. The DRV8711 functionally more advanced, with up to 256 microsteps, stall detection. DRV8711 uses external MCU for motion profile vs. L6482HTR has built in.
Regards, Murugavel