This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H- BRIDGE FOR motor driver

Guru 13485 points
Other Parts Discussed in Thread: DRV8800, DRV8802, DRV8832, DRV8833

Looking for  H-bridge for motor/valve drive – 2x N-Channel and 2x P-channel FET. ~600mA

  • Eli,

     

    Not sure what your voltage is, but we have several options:

    DRV8800/1: 1.5A continuous, single H-bridge driver, 8V-36V

    DRV8802: 1.1A continuous, dual H-bridge driver, 8.2V-45V

    DRV8832: 1A continuous, single H-bridge driver, 2.75V-6V

    DRV8833: 1.5A continuous, dual H-bridge driver, 2.7V-11V

     

    If you need something different, please provide more details.