This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3946-Q1: Command without SPI

Part Number: DRV3946-Q1


Hello, 

Is it possible to Enable/Disable the driver outputs without using SPI commands ? only using EN1/2 pins ? 

Thanks.

  • Hey Rachid,

    You can configure it to use EN1/EN2 to turn OFF the driver. PIN_CONFIG settings determines the function of the two pins.  w.

    The Chx_CTRL bits in CMD1 register must be programmed appropriately to turn ON the driver. 

    You will also need SPI for device configuration no matter what.  

    Best,

    Jacob