Hi team,
I received some questions. Customer is concerned about are there any problems with the way using the device following.
Could you support these please?
- If the fault pin is not used, is it OK to go directly to GND?
- When power on, 3.3V(for STEP,ENABLE,DIR,SLEEP) is applied earlier than 24V(VM). is it OK?
- To avoid momentary excitation when the system power up,
ENABLE is pulled down by 10k Ω so that the EN pin is around 0.1 V at start-up. is it OK?
Best regards,
Goto