Part Number: DRV8873-Q1
Hi Experts,
DRV8873-Q1 is mass production on customer side. Could you confirm the meaning of those register? Thanks.
For OCP, there only one parameter show the OCP, Iocp= 10A, and the Tocp= 5us. But I find there are 2 faults for one half bridge: OCP_H1 and OCP_L1, for those two faults bit, does it mean that:
OCP_H1: means the current on the high side FET bigger than 10A.
OCP_L1: mean the current on the low side FET bigger than 10A.
Itrip which mean the current limit threshold that wouldn't trigger the OCP, the Itrip can be configured by SPI, In my understanding, Itrip and Iocp are two different parameters. Is it right?
I also want to know: Is there any relationship between Itrip and OCP_H1/OCP_L1? Thanks.
Best Regards
Songzhen Guo