This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243-Q1: diagnostic logic

Part Number: DRV8243-Q1


Hi,

When running in PH/EN mode, do the following faults comply with the chip's own diagnostic logic?
1. Forward rotation, EN=20%duty, OUT2 short to ground, chip reports H2_OCP fault;
2. Reverse rotation, EN=20%duty, OUT1 short to ground, chip reports H1_OCP fault;

Thanks!

  • Hi Mingkang, 

    May I know what is the concern with the observation? A short to GND on OUTx will result with over current via the conducting HS-FETs. So a global OCP along with the corresponding HS-FET OCP fault, either H1_OCP or H2_OCP fault as qualifiers will be reported in the SPI control devices.

    Regards, Murugavel

  • Yes, you're right.  Will the observation be the same under the condition of EN=20%duty?

  • Hi Mingkang, 

    Yes. Technically it should be the same. When the short happens while there is current recirculation (high-side) during PWM off time the motor could change direction depending on which OUTx was energized and which OUTx was shorted. This may complicate behavior. But in general the HS-FET OCP fault will occur for a OUTx to GND short even with 20% or lower PWM duty cycle. You can test this with an EVM. 

    Regards, Murugavel