Hello all,
I am finalising a design based on the DRV8402 and DRV8432. The 8432 would be the preferred part but availability concerns means I have to design for the 8402 as well. Factory fit options for supporting component such as OC_ADJ resistor is fine.
I have a couple of questions:
1) AGND-GND connection
The 8432 suggests a 1 ohm resistor to provide a little isolation between AGND and GND (pins 8 and 9). The 8402 does not have this. Would it present a problem if the 8402 build had the 1 ohm resistor? Or alternatively we could easily enough fit a 0R for the 8402 variant. Any problem with this?
2) Output protection
My application has long cable runs (up to 40 metres) that go to externally mounted motors. These are isolated from direct weather but normal "outside" problems can be present - lightening mainly. Wiring is floating but induced currents could be significant. I am not expecting to protect against direct strike to the (pole mounted) systems. I would like to provide reasonable level of protection.
Unidirectional 1500W transient suppressors in an SMC pkg from each output to GND would be a start, possibly also DIN rail mounted lightening surge arrestors (but possibly too slow to be of huge benefit). Would the single diode drop breakdown in the reverse direction present any problem? It will appear in parallel to the low side MOSFETs body diodes. Which raises the issue of whether the tansient suppressors should go on the inboard or outboard side of the current-limiting inductors. I am thinking inboard side.
I will probably be including fusing as well (resettable or PCB mount .. not sure yet) but this will mainly be to catch load wiring errors as an adjunct to the cycle-by-cycle limiting of the chip.
Motor supply is 48V regulated. Most of the motors (this is multi-channel) will be driven in simple full-bridge mode. A few will need higher current and will be driven in parallel full bridge mode. Motor control is not needing to be very precise in this application. I will be being very generous in the bulk PVDD decoupling caps (more than EVM) and the local 100nF decouplers will be very close to the chip. I was going to make provision for snubbers (3.3R+10nF) from each output to ground (on the external side of the current limiting inductors).
Would the transient suppressors cause any issue? Inboard or outboard side?
Any suggestions on anything more I can do to increase reliability?
Thanks,
Ian