Part Number: DRV8833
Other Parts Discussed in Thread: DRV8881
Hi everybody,
In a previous question i asked some questions about the possible values for Rsense on this IC.
I assumed that once the current through the motor exceeded the set limit (Ichop), the nFAULT would be pulled low.
However in practice this did not seem to happen.
Is it true that Rsense is used to set the current control circuit which fuctions as a torque limit circuit.
And, that nFAULT only is pulled low whenever the Iocp (2 - 3.3A) is reached?
This would mean nFAULT cannot be used as a stall detection signal.
Thanks in advance for clarifying.
Simeon.