This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8462EVM: GUI and EVM doesn't work

Part Number: DRV8462EVM


Hi,

I have installed the DRV84xx_DRV82x2_DRV89x2-EVM-GUI but I couldn't start it.

What could be the reson?

I have connected the EVM with the PC and I also have connected a stepper motor and 24 VDC to the board

The LED for 3V3 and that for VM is on. But there is no voltage on the DVDD output.

What could be wrong?

Thanks a lot

Albert