Other Parts Discussed in Thread: DRV8412
Dear TI experts,
My customer considers DRV8262 for their new project. and They have some questions as below. Could you check these questions?
1. Can My customer use DDV package of DRV8262? (I can see only DDW package in product page.)
2. What is the meaning of DC on the table below? Is it not a pulse, contimuous load?

3. Is OCPM pin just determine the type of recovery? (latch-off type recovery=low or automatic recovery=high) Anyway My customer should determine this pin set high or low. right?
4. About overcurrent protectoin, Can I adjust the value of overcurrent detection? (DRV8412 has OC_ADJ pin and I can program the value using resistor.)
5. THey will connect peltier to the output of DRV8262 in single mode.
Can I use all out 1 pin tie together (P4,P5,P6,P17,P18,P19) and use only 1 inductor? or use 2 inductors? (P4,P5,P6 and P17,P18,P19 separately)
6. When I use IPROPI pin in sigle mode, Can I recognize foward current or reverse current?
7. My customer will use 200KHz frequency for PWM mode. Is there any concern for schematic?
Best regards,
Chase