Other Parts Discussed in Thread: STRIKE, DRV110, DRV8846
We are using the DRV104PWPR chip and trying to drive a 8watt air solenoid with a 24VDC turn on for 8 ms and then drop the voltage to about a 40% duty cycle. I have the circuit diagram attached and it is setup like the datasheet example in Figure 17. When we have no load connected, the output acts as expected, where we have 24V for about 8 ms then it chops to an average of 9.7VDC. But when I connect a load, the voltage during chop reduced to an average of 2.4VDC. Do you have any idea what can be causing this?