This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8871: DRV8871

Part Number: DRV8871
Other Parts Discussed in Thread: , DRV8251A

Hello, I'm encountering an issue with the DRV8871 motor driver and would appreciate some insight. I've been testing it with a DC motor and experimenting with the current limitation by adjusting the Rlim value according to the formula provided in the datasheet: Ilim = 64/Rlim. I've tried various current limitation values ranging from 2A to 4A.

However, after several tests and manipulations, particularly at higher currents, the driver starts emitting a sound similar to that of birds and I've also noticed a ticking sound. Additionally, it heats up very quickly.

Has anyone else experienced similar issues or have any suggestions on how to address this problem?

Thank you in advance for your help!