This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8462EVM: DRV8462EVM

Part Number: DRV8462EVM
Other Parts Discussed in Thread: DRV8462

Hi,

Can I please receive help to program the DRV8462 EVM using the scripting function to go forwards until stall and then reverse until stall for a calibration step and then use the step counts as a means to change direction and not stall detection? the reason is because the stall detection as a method to change direction for calibration is fine (to determine the number of counts until end position) but as a long lasting method our solar cleaning robot will be damaged as the stall impact is a lot over time. 

Kind regards,

Phillip Bothma