Part Number: DRV8214
Hi,
Please take a look at the following problems. The customer is considering how to keep the torque unchanged while regulating speed, instead of decreasing the torque as the speed decreases and increasing the torque as the speed rises.
In the speed regulation mode, is the voltage at both ends of the motor stable or changes with the speed change?
If the voltage is changing, is the motor torque also changing, the lower the speed, the smaller the torque?
Thanks~