This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8714-Q1: SPI Clock Fault

Part Number: DRV8714-Q1


Hi Team,

The DRV8714 SPI clock should be 16bit. While we sent 32bit clock in one nSCS, will this trigger the SPI clock fault?

During the test we didn't received the SPI clock fault indication.

May I know what is the definition of the 'Invalid SPI Lock Frame' ?

Thanks!

Best,

Frank

  • Frank,

    Did they read the register or just monitor nFAULT?  Per the description below, SCLK_FLT is NOT reported on the nFAULT pin.

    Also, was the data recognized by the device?  In other words, was the register they were attempting to write to updated?  Data should have been ignored.

    Regards,

    Ryan

  • Hi, Ryan,

    1. We have read the register, not monitor the nFAULT. In such case, the bit SPI_OK of register IC_STAT1 is always 1. 

    2. The data can be written and read correctly from the device.

    In the picture, you can see that the time between two 16bit clock is about 1.2us. We want to know the  SCLK_FLT was not set is related to it(1.2us).

    And we want to know all the conditions that can leads to SCLK_FLT. At least currently, we sent 32bit clock in one nSCSwe hasn't trigger SCLK_FLT.

  • Hey Ronglai,

    1.2us is much more than the required SCLK minimum period of 100ns, so that time should not be the issue.

    Can you post a scope capture of a single SPI transaction (16 bits) more zoomed in? The clock signal looks wavy in your capture above.  

    Is this on your PCB or on our EVM?  If EVM, how long are the SPI jumper wires MCU-EVM?

    Best,

    Jacob

  • We used a logic analyzer to examine the data. The first 16bits data are normal. The response  of the second 16bits data is random. Can we assume the firt 16bits data were recieved and responded correctly and the second 16bits data were ignored?

  • Hey Ronglai,

    Please give our expert on this device another day to look into this.  

    Can we assume the firt 16bits data were recieved and responded correctly and the second 16bits data were ignored?

    Per the datasheet, SDI pin receiving more or less than 16 bits should cause a SCLK_FLT and the entire transaction to be ignored.  You've confirmed that SCLK_FLT isn't triggering after the transaction, and that the transaction is successfully writing to the device?  Just want to make sure we understand the question correctly.  

    Could you test it with less time between the two strings of 16 clock pulses?  

    Best,

    Jacob

  • Could you test it with less time between the two strings of 16 clock pulses?  

    You can see that the response data is different when read the same register(IC_STAT1) using less time between the two strings of 16 clock pulses.

  • Hey Ronglai,

    Hmm interesting. I have posted this to our design team and will let you know what they say, though fair warning it might be a few days.  

    Can we assume the firt 16bits data were recieved and responded correctly and the second 16bits data were ignored?

    If this is what your testing is showing, I am comfortable saying Yes to this question.  Test it first by 1. Read all registers 2. Write to a register.  3. Read all registers and confirm that only the register you wrote to was changed.  Test that on a few registers, and if that checks out then I'd move forward with that conclusion for now unless I can get a more definitive answer.

    Best,

    Jacob

  • OK, waitting for your reply. Our customer is very concerned about the result.

  • Hi Ronglai, 

    Thank you for your patience. We will update you as soon as we can.

    Best,

    Keerthi

  • Hey Ronglai,

    I heard back from Design:

    In RTL it looks like first 16 bits are ignored and last 16 bits are received. SPI frame with 32-bit clock pulses are not safe it could corrupt register data as in last 16 bits.

    Need to check in RTL simulation to double confirm this issue in the SPI interface IP. We do not have simulation ready right now. It will take some time.

    We could confirm in EVM/test-boards by reading data send in 4th byte from register address pointed by 3rd byte.

    Could you have the customer try to test this bold section?  I don't have the bandwidth right now to dig into this EVM to make custom firmware for 32-bit SPI, but seems like customer has this already.  

    Thanks,

    Jacob