Other Parts Discussed in Thread: DRV8245-Q1, DRV8244-Q1, DRV8144-Q1
Hi,
Our application requires to run motor at 10A for 0.5 ms. We ran into a problem where the total output current from a custom board with DRV8243HQRXYRQ1 limits the output current to around 7A (@8V). Physically bypassing the drive allows to run the motor at 10A. ITRIP pin of the motor is grounded so current limiting should be disabled.
Reading the nFAULT pin the drive overheats after 3-5 seconds running at 7A, and pulls the pin low. Regardless of this the first seconds the drive seems to operate normally except the current issue.
Any suggestions to try, before switching out the drive?