Hello team,
I want to know the detail of Full-scale current accuracy of +/- 4% from the datasheet.
Is this indicating Current trip accuracy of +/-4%?
I want to use DVDD as VREF from resistor divider.
Is this current trip accuracy (±4%) including the DVDD accuracy (5V±0.25V) and resistor error of ±1%?
OR should I add those errors in to account?
Best Regards,
Kei Kuwahara