Hi,
I am using the DRV8353RS-EVM to operate the BLDC motor, and I am controlling the motor speed using the GUI. I pressed the RESET switch S2 (FSMJSMA), and the EVM board began signalling the fault. I then tried to connect it to the GUI to operate the motor, but the motor was not functioning, and the EVM board indicated the fault Signal.