Other Parts Discussed in Thread: DRV8874
Hello Team, one question from customer:
Is the charge pump active when OUT1 and OUT2 are tri-state (means in-acitvie) ?
Many Thanks
Josef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team, one question from customer:
Is the charge pump active when OUT1 and OUT2 are tri-state (means in-acitvie) ?
Many Thanks
Josef
Hi Josef,
Who is the customer and what is their application? The charge pump will still be active even if the outputs are HI-Z'ed. What is the reasoning behind this question?
Best,
Keerthi
Hi. We were thinking about to use the charge pump of the DRV8874 to control a transistor which is in series with OUT2. The purpose of this transistor is to avoid a current flow backwards through the bulk diode of OUT2. Between OUT2 and the transistor, we have a shunt to measure the current, but this current measurement has to be calibrated. For this calibration process we need to put OUT2 in HI-Z'ed but we still have to activate the transistor.
Hey Georg,
Agreed with Keerthi, the charge pump will still be active when OUTx is Hi-Z. So sounds like that should work for your system. I recommend seeing if you can modify a DRV8874-Q1EVM and testing it out there, seems like it should work.
FYI, the body diodes of our FETs are rated for the same amount of current as the FET itself, so this type of extra protection is not typically necessary.
Best,
Jacob