Hi
I am considering using the DRV8838 H bridge driver, the application is battery operated with a long service life so sleep current is important.
From the data sheet the sleep current is specified at 120nA through Vm + Vcc. However the logic low input current with Vin = 0V is specified at
5uA max. It is not clear if total system sleep current is 120nA + 15uA max with the 3 digital inputs when in sleep mode. Can you clarify please.
Thanks