I am using the DRV8353RS and have checked via SPI communication and only the GDUV error signal is active.
The rest of the signals are consistent with the datasheet. However, I have a picture like the one in the datasheet and looking through it, it looks like the activation is correct. I would be grateful if you could confirm this.

I checked that the PWM signal applied to the DRV8353RS through the DSP is normal, and the PWM output is normal when the motor is not connected, but when the motor is driven, the motor driver or mosfet is damaged.
So far, only phase A is being corrupted and I was wondering if you have any data on this phenomenon. Do I need to change the IDRIVE settings in this case?