This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8701: Regarding DRV8701 PSPICE for TI waveform

Part Number: DRV8701

Hi,

In attached DRV8701 TI PSPICE output waveform with all default settings ,18V 6mA profile Vgh2 is expected to be 0V but it is High for some time.

  • Hi Pritesh,

    Your inquiry is under review. 

    Please allow until Monday for a response.

    Best,

    David

  • Hi Pritesh,

    Can you tell me what the inputs are in the "default" mode? 

    Are you in PWM mode and sending PWM signals to both inputs (IN1 & IN2) or PH/EN mode?

    From the waveforms it looks like you are switching between FWD and BRAKE (slow decay) which is a normal operation. However, I am not sure of the spike on GH2. I have tested on an evaluation module in the lab, and could not reproduce the behavior in PH/EN mode switching from FWD to BRAKE (slow decay). 

    Best,

    David