Other Parts Discussed in Thread: DRV8803, DRV8932
Hello
I was looking at the DRV8860 for a solenoid control application - I hit the solenoid with 100% duty cycle and then hold a 50% duty cycle. But, I need the solution I choose to have a switching frequency between 20 and 40 kHz. According to the below snippet from the datasheet, this device will be operating at 50kHz when the duty cycle is >25% (which is all the time in my application).
Question: Is there a different device that operates in my desired frequency range and has similar functionality to the DRV8860?
Thanks!