This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8245-Q1: IPROPI Sense and equation

Part Number: DRV8245-Q1

Hi all, 

I'm developing the board which used DRV8245. I have some questions about IPROPI usage and equation.

I've read this [How to configure IPROPI and current sensing] but still not sure and need to recheck my understanding.

7.5.8 IPROPI & ITRIP Regulation

For HTSSOP package, It said that [A_IPROPI is 6150 A/A]. Is it means that the Output current at IPROPI pin of ICs is equal to the current sensed at internal High-side FET divided by 6150 in Amp.

Then, To make IPROPI be readable by ADC, it's up to suitable Rsense. For instance,

If Motor current is in range [0, 10]A / 12-bit ADC in range[0, 3.3]V., 

Vout to ADC = Ipropi x Rs

3.3 = (10/6150) x Rs

>> Rs (implement into the board) is about 2KΩ. 

Then, to calculate read value from ADC back to Motor's current (I_motor), uses this equation:

MotCurVolt = [(ADC_raw / 4096) x 3.3]

I_motor = [MotCurVolt / 2000(Ω)] x 6150

Is my understand correct?