Dear person in charge,
What does it mean when the reserved bits 28 and 29 of GD_CONFIG1 are checked?
If the reserved bits 28 and 29 are not checked, GD_CONFID1 = 0x0006807B, but if they are checked, GD_CONFID1 = 0x000680FF. In this case, is there any error that is not mentioned in the MCT8329A datasheet? I would like to know the difference between these setting values.
I have a feeling that the presence or absence of this reserved bit changes the occurrence of the fault.
Translated with DeepL.com (free version)