Hi,
We have used DRV8845RHHR in our project to drive stepper motor having following specifications.
1) No of phase - 2
2) Phase voltage - 6.6V
3) Phase current - 1A
4 ) Phase resistance - 6.6ohms
5) Size : NEMA 17
The applied voltage on VM1 and VM2 pins is 11.5V.
The VREFX reference voltage pins are connected to PWM outputs of microcontroller for which the VOH logic level is 3.3V.
We have used voltage divider ckt and adjusted VREF voltage of 1.47V on all VREFX pins.
All sense pins have 0.47 ohms 1 watt resistor to GND.
The maximum itrip calculated is ITRIPMax = VREF / (3 × RSENSE)
= 1.47/(3 x 0.47)
= 1.04A
The maximum power to stepper motor is 6.6W as mentioned in the above motor specifications.
How much PWM duty cycle should be set on Vrefx pins to limit the maximum power of 6.6W to motor with above stepper motor specifications?
Also provide calculations for the same.
Regards,
KIRAN SURVE