Other Parts Discussed in Thread: MSP430F5528, MSP-FET
Hello, I meet a problem when using DRV8262EVM.The status is that the D2 led cannot light on.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I meet a problem when using DRV8262EVM.The status is that the D2 led cannot light on.
Hi Zhiyu,
If the MCU STATUS LED is not blinking try performing a firmware reset using the push button S1 with jumper J27 in 1-2 RST position.
Best,
David
Hey Zhiyu,
Please see this FAQ: [FAQ] Why won't my Motor Driver EVM connect to the GUI?
In this case please confirm you 1. Plug in Micro-USB to PC 2. Turn on VM power supply >5V. Maybe wiggle the micro-USB connector in case it is loose or not making good connection?
Make sure the jumpers are installed here:

Then in the GUI do File, Program Device to flash latest firmware onto the EVM
Best,
Jacob
May be the MSP430F5528 is broken,we try to replace the MSP430F5528,can you give me a guide on how to program MSP430F5528 and send me a programmer file .
Hey Zhiyu,
Can you probe the 3.3V test point to see if there is 3.3V?
For flashing the EZFET firmware onto the top MDP430F5528, if you have a MSP-FET see the attached info:
7651.Programming a blank MSP430F5528 in the Brushed and Stepper motor driver EVMs.zip
Got it from this post: https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1311649/drv8262evm-unable-to-recognize-usb-port-after-fw-update/4984304#4984304 I am not sure why we are having issues updating only this EVM.
Best,
Jacob