This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: MCF8316C_Torque Mode

Part Number: MCF8316A


hi,

Q1:Is there a register that can read the speed mode or torque mode status?

Q2:Why is it useless to change PWM control when the motor loses control in speed mode when modifying SPEED-LOOD0DIS=1 torque mode?

  • Hi,

    Q1:Is there a register that can read the speed mode or torque mode status?

    You can see the state of the algorithm by referring to the ALGORITHM_STATE register.

    If you would like to know what speed/current value the algorithm is targeting while in the speed/torque loop modes you can refer to SPEED_REF_CLOSED_LOOP register for the speed reference when the device is in closed loop and IQ_REF_CLOSED_LOOP register can be referred to to see the current being targeted.

    Q2:Why is it useless to change PWM control when the motor loses control in speed mode when modifying SPEED-LOOD0DIS=1 torque mode?

    Would you mind providing me more information on the issue you are seeing and what registers you are modifying?

    Regards,

    Joshua