I already have the DRV3901EVM board and have primarily tried to establish a connection with the GUI via the Internet browser. I installed the Chrome extension and the TicloudAgent application. I have also installed the msp430 driver. It also recognises the two Com Ports (UArt) in the Device Manager and Texas Instrument is also listed as a driver manufacturer.When I press Connect in the Internet GUI, the connected com port is displayed, but it always fails to establish the connection. I have also tried it with a private PC, which has no firewall or similar. I then tried to install the GUI on the PC (DRV3901-Q1EVM-GUI-1.1.1.setup-win), but this did not work. It cannot find the files it wants to download from the Internet.