Hi,
As the title states, my question is regarding the NC pins 22-25 on the motor driver IC. They are stated as No Connect without any (that I could see, please tell me if I've missed it somewhere) indication that they should be tied to anything. Yet in the Evaluation Module (which is also shown as a layout example on the datasheet) they are tied to AGND.
I'm designing a custom board for this IC and trying to understand what the guidelines are regarding these pins. Any clarification on what the implications of leaving these floating vs having them tied to Analog Ground are would be much appreciated.
Many thanks,
Arvids