Tool/software:
Hi team.
What are the requirements for waveforms that can be applied to Vinx?
As far as I can see from the diagram below, I believe that if Vinx does not output Hi for at least the following total time, the upstream or downstream FET will be half-ON.
"tPD"+"Fall time of VGSLx"+"tDEAD"+"tDON"+"Rise time of VSHx from VSHx_L to VSHx_H"+"tPST_CHR"
Do you agree with the above idea?
Also, in that case, where is the "tPD" time defined?