This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8215: Brushed DC Motor Driver

Part Number: DRV8215
Other Parts Discussed in Thread: DRV8837

Tool/software:

Hello,

I am looking for an IC to control a 3V Brushed DC motor, maximum current in stall is about 100mA.

  • The motor should have current control on the motor, being able to cut the power supply when it exceeds a previously configured limit.
  • It must be able to control the motor in both directions. Selected using two switches.
  • System powered by 3.7V battery. Battery charging could be managed by an external module.

I would appreciate any suggestion.

Thanks in advance.