This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8701: DVDD (3.3V LDO) 0V

Part Number: DRV8701


Tool/software:

 I have used the DRV8701 in the past with much success, but this is the first time I have attempted to the DVDD 3.3V LDO as the primary supply for my design. I cannot measure any voltage on the DVDD pin.

I did made a mistake in the layout enabling the nSleep pin but have since severed it during this investigation (red) . Additionally, I have severed (red) the DVDD pin to ensure there isn't a something drawing the DVDD pin down. I am not stumped.

I can measure the supply voltage, 9.6V at VM 

I did have the board populated at a fast-turn internet supply, I will be ordering some DRV8701 this weekend to ensure there isn't a counterfeit situation happening, but I suspect this not the case.

Any help would be appreciated,