This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3946-Q1: Optimum driver for solenoid valve pulsing in 50-150Hz frequency range and with 0-100% dutycycle control

Part Number: DRV3946-Q1

Tool/software:

Hi. I am searching for an optimal driver that controls the opening and closing of a small 24V 500mA solenoid valve and wondering if the driver can handle that device at maximum 24V and 12mA

Thank you so much bestregards

  • Hi ,

    Thanks for the question,

    The lowest PWM frequency programmable for DRV3946-Q1 is 500Hz. Is this OK ffor the application.

    Further, could you help me the some more details on the end application

    1. What is the absolute max voltage and maximum operational voltage?

    2. Would the application need any current control or just duty cycle programming is enough.

    Thanks,

    Ibinu