This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983-Q1: questions about application

Part Number: DRV10983-Q1

Tool/software:

Hi team,

For DRV10983-Q1 application, here are 2 questions need your help. Motor parameter: Phase resistance is 36Ω, 6 slots and 8 poles, Y-type winding, inductance is 33.8mH.

Question 1: The phase resistance exceeds 18.5Ω, which is not within the range of "Table 3. Motor Phase Resistance Look-Up Table". Is DRV10983-Q1 suitable for driving this motor?
Question 2: When using DRV10983-Q1 to drive a brushless DC motor, which parameters of the brushless motor must be within the "DRV10983-Q1" specification range?

BR

Jiawei