This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8718-Q1: Low IQ powered off braking off function

Part Number: DRV8718-Q1

Tool/software:

Hi Team,

We have some general questions relate to the DRV8718-Q1 low IQ powered off braking function.

1. Right now we are achieving the POB function with external OV detect, while there is internal OV detect inside the DRV8718 as well. Is it a good idea to remove the external OV detect and use internal OV detect? Will this internal fully support the low IQ braking function?

2. According to datasheet, the POB can only enable when low-power sleep mode(nSLEEP=LOGIC LOW). What will DRV8718 react when nSLEEP=logic high and Brake=logic high? 

Thanks,

Best,

Frank