This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8714-Q1: Can this device drive a brushless motor like TLE92104?

Part Number: DRV8714-Q1


Tool/software:

e2e, 

Can DRV8714-Q1 drive a brushless motor like TLE92104?

Thank you,

Adam 

  • Hey Adam,

    Yes, it could.  You would use the device in independent 1/2 bridge control mode and use 3 1/2 bridges for the BLDC motor.  You would have to manually implement the BLDC commutation pattern and use external MCU to read the hall sensors of the motor.  

    If your only load is a BLDC motor I recommend looking at TI's BLDC motor driver portfolio instead.

    Best,

    Jacob